I am looking at adding a USB to a MCF51jm 128. Looking through this forum I found a few references to MQZ and this AN, but they will several years old. Has anyon tried AN39277 and current tools?
Any comments or suggestions?
Thanks
已解决! 转到解答。
Hi Barber,
Good timing of question. I've just helped someone else get this running with FSLMQX3.7 and M52259DEMO.
I found issue that I haven't found the root cause of yet but did find workaround to get the jump table working correctly.
I simple created a new "C" file to contain:
asm void jumptable(void);
extern unsigned long __boot;
#pragma define_section jump_rom ".jumprom" far_absolute R
__declspec (jump_rom) asm void jumptable(void)
{
nop
jmp __boot
}
Then added it to the application I want to load into FLASH.
The linker is updated with the following:
MEMORY
{
jumprom (RX): ORIGIN = 0x00004000, LENGTH = 0x00000010
...
KEEP_SECTION { .jumprom, .vectors_rom, .vectors_ram, .cfmconfig }
.jumprom :
{
___JUMP_ROM_START = .; # Jump table
jump_rom.c(.jumprom)
. = ALIGN (0x4);
} > jumprom
Lastly with the above changes you DO NOT need to have the following code used:
#pragma define_section jump_rom ".jump_rom" far_absolute R
__declspec(jump_rom) const unsigned char _UserEntry[] @ USER_ENTRY_ADDRESS = {
0x4E,
0x71,
0x4E,
0xF9 //asm NOP(0x4E71), asm JMP(0x4EF9)
};
__declspec(jump_rom) void (* const _UserEntry2[])()@(USER_ENTRY_ADDRESS+4)=
{
__boot,
};
This is the code snippet that doesn't seem to be working as it did with the older CW7.1. But I think my workaround is a bit more straightfoward and understandablle...at least to me.
I'm currently at a week long training event and will look to get Appnpte and other documentation generated to help others.
Hope this helps.
Regards,
David
PS
Trying to attach a ZIP that has the files I modified for my projects but if it doesn't show up its because I seem to had issues with getting attachments to load.
Hi Barber,
Good timing of question. I've just helped someone else get this running with FSLMQX3.7 and M52259DEMO.
I found issue that I haven't found the root cause of yet but did find workaround to get the jump table working correctly.
I simple created a new "C" file to contain:
asm void jumptable(void);
extern unsigned long __boot;
#pragma define_section jump_rom ".jumprom" far_absolute R
__declspec (jump_rom) asm void jumptable(void)
{
nop
jmp __boot
}
Then added it to the application I want to load into FLASH.
The linker is updated with the following:
MEMORY
{
jumprom (RX): ORIGIN = 0x00004000, LENGTH = 0x00000010
...
KEEP_SECTION { .jumprom, .vectors_rom, .vectors_ram, .cfmconfig }
.jumprom :
{
___JUMP_ROM_START = .; # Jump table
jump_rom.c(.jumprom)
. = ALIGN (0x4);
} > jumprom
Lastly with the above changes you DO NOT need to have the following code used:
#pragma define_section jump_rom ".jump_rom" far_absolute R
__declspec(jump_rom) const unsigned char _UserEntry[] @ USER_ENTRY_ADDRESS = {
0x4E,
0x71,
0x4E,
0xF9 //asm NOP(0x4E71), asm JMP(0x4EF9)
};
__declspec(jump_rom) void (* const _UserEntry2[])()@(USER_ENTRY_ADDRESS+4)=
{
__boot,
};
This is the code snippet that doesn't seem to be working as it did with the older CW7.1. But I think my workaround is a bit more straightfoward and understandablle...at least to me.
I'm currently at a week long training event and will look to get Appnpte and other documentation generated to help others.
Hope this helps.
Regards,
David
PS
Trying to attach a ZIP that has the files I modified for my projects but if it doesn't show up its because I seem to had issues with getting attachments to load.