Now Available: CyaSSL for MQX RTCS – Enabling Secure Network Connections for Kinetis MCUs
We are pleased to announce the availability of the popular CyaSSL SSL / TLS software library in a pre-configured commercial-evaluation add-on package for Kinetis SDK v1.1.0 (and later).
In just a few extra steps, you can enable secure network connectivity with CyaSSL in MQX Real-Time TCP/IP Communication Suite (RTCS) examples.
Installers for Windows and Linux are available. CyaSSL version 3.2.0 (or later) included.
Description
The CyaSSL embedded SSL library is a lightweight SSL/TLS library written in ANSI C and targeted for embedded, RTOS, and resource-constrained environments - primarily because of its small size, speed, and feature set. CyaSSL supports industry standards up to the current TLS 1.2 and DTLS 1.2 levels, is up to 20 times smaller than OpenSSL, and offers progressive ciphers such as HC-128, RABBIT, NTRU, and SHA-3. User benchmarking and feedback indicates dramatically better performance when using CyaSSL over OpenSSL.
Key Features
* - Accelerated throughput available via the Memory-Mapped Cryptographic Acceleration Unit (MMCAU) on select Kinetis MCUs.
* - Accelerated throughput available via the Memory-Mapped Cryptographic Acceleration Unit (MMCAU) on select Kinetis MCUs.
Key Derivation (HMAC, PBKDF2, PKCS#5), Key Generation (RSA), Signed Certificate Generation (x509 v3 RSA and ECC), PEM and DER certificates, Private Key Encryption (PKCS #8, #5, #12), Elliptic Curve Cryptography (ECDH-ECDSA, ECDHE-ECDSA, ECDH-RSA, ECDHE-RSA), Online Certificate Status Protocol (OCSP), Certificate Revocation List (CRL), IPv4, IPv6, and more.
More details at CyaSSL Embedded SSL Library Product Details
Licensing
Through our partnership with WolfSSL, Freescale is providing a free commercial evaluation version of CyaSSL for Freescale customers to use for internal development, testing, and evaluation purposes. Customers who wish to incorporate CyaSSL into proprietary appliances must obtain a commercial license from WolfSSL, which is available at a very reasonable cost.
For additional information on licensing, see WolfSLL License Information.
Hardware Supported
Project build files are provided for the following Freescale evaluation boards:
FRDM-K64F
TWR-K64F120M
TWR-K60D100M
Example Projects Provided
HTTP Web Server - Access the board with a web browser using an authenticated and encrypted connection.
How to Get Started
1. Download Kinetis SDK v1.1.0 (or later) at www.freescale.com/ksdk
Click Download.
Choose the appropriate Kinetis SDK installer for your operating system, then download and install it.
2. Now install CyaSSL for Kinetis SDK with MQX RTOS
On the left side of the same download page, click Updates and Patches
3. Choose the appropriate CyaSSL installer for your operating system, download and install it.
CyaSSL source files will be installed within the <Kinetis SDK>\tcpip\rtcs\source\ssl\ folder in the Kinetis SDK directory tree.
On Windows, this path is typically: C:\Freescale\KSDK_1.1.0\tcpip\rtcs\source\ssl
4. Check out the _readme.txt file at <Kinetis SDK>\tcpip\rtcs\source\ssl to see how to run the example projects provided and to see how to add CyaSSL to your projects.
More tutorials to come.
Best of luck with your connected embedded projects!
Mac Lobdell
Freescale Software Technical Marketer
Hi,
i am not getting CyaSSL for Kinetis SDK v1.1.0 with MQX RTOS download option.
am getting only SDK v1.2.0 but i am using KSDK V1.1.0 am already tried some example using V1.1.0. can you give exact link for download CyaSSL for Kinetis SDK v1.1.0
thanks and regards,
sudhakar p
Hi,
The cyaSSL patch for "MQX RTOS for KDSK v1.1" is available at www.freescale.com/mqxrtos<http://www.freescale.com/mqxrtos>. Click the big download button on the first page, then log in. This will take you to the MQX enablement software downloads portal. Click the "Previous" tab. Cyassl is on the top of the list.
Thanks,
Mac
FYI
A cyaSSL patch for "MQX RTOS for KDSK v1.2" is available at www.freescale.com/mqxrtos<;http://www.freescale.com/mqxrtos>. Click the big download button on the first page, then log in. This will take you to the MQX enablement software downloads portal. Click the "Previous" tab. Cyassl is on the top of the list.
Thanks,
Mac
Hi Sean,
I'm part of the wolfSSL engineering team. If you download wolfSSL (formerly CyaSSL) direct from the wolfSSL website, we include some example CodeWarrior project files under the <wolfssl_root>/mqx directory, specifically:
wolfcrypt_benchmark
wolfcrypt_test
wolfssl
wolfssl_client
These have been put together for CodeWarrior, MQX, RTCS, and MFS, on the TWR-K70F120M board. They may be insightful as to how to use wolfSSL/CyaSSL from CodeWarrior. The README located at <wolfssl_root>/mqx/README should be helpful as well.
Best Regards,
Chris