I have ported my application from CodeWarrior to KDS. It works just fine, except I can not get the MQX plugins to work. All of the MQX views "Task List", "Lightweight Memory Pools" and so on show "Task list not retrieved successfully!"
And my call stack only shows one task, when in CodeWarrior it would show the stack for each task. What am I missing? I have read all of the documentation I can find but nothing.
KDS V 2.0.0
MQX Lite 1.1.1
已解决! 转到解答。
Hi Leif!
I have good news for you!
The issue was fixed (TAD version 1.0.8) and will be available on KDS update site along with release of KDS 3.0.0.
It is expected by end of April/beginning of May
Kinetis Design Studio Integrated Development |Freescale
Have a great day!
Kind Regards,
Iva
Thanks Iva,
more notes
It worked once or twice, but does not any more. The code I am working with has changed very little, and not at all in the PE, or generated code areas.
But when it did, it was very very slow.
Just tried removing it and re installing the plugin, it worked during the first debugging session. But not the second.
Hi Leif!
I have good news for you!
The issue was fixed (TAD version 1.0.8) and will be available on KDS update site along with release of KDS 3.0.0.
It is expected by end of April/beginning of May
Kinetis Design Studio Integrated Development |Freescale
Have a great day!
Kind Regards,
Iva
Hi Iva,
I'm using KDS 3.0.0, KSDK 1.2.0, and have the latest TAD installed (1.0.8.201504151538) but I am also having this same problem.
Nothing is showing up in the TAD windows. For example the MQX Task List tab shows "Task list not retrieved successfully" in the Task Name column. Any idea what the issue might be?
Thanks,
Peter
....Just discovered that these fields only show up after I hit the pause button..., progress...
Hello Peter Furey and Leif Zars,
if you want to see the MQX Task List, you should suspend it by the button
then you will see in MQX Task List
Please, does it help you?
Best Regards,
Iva
Hello Leif!
Thank you for your feedback.
Kernel log should show only one log - kernel log.
Please, tell me your board, what do you use for project? which version of MQX are you using?
You can also attach the screenshot of the issue.
Best Regards,
Iva
Hi Leif,
Things to try:
- Re: Problem: Installing MQX RTOS Task Aware Debugger for GDB plug-in (TAD)
-
According to this the MQX_init_struct should contain fake items for START_OF_KERNEL_MEMORY and END_OF_KERNEL_MEMORY.In the MQX examples the structure looks like this:
Try to comment out the START_OF_KERNEL_MEMORY and END_OF_KERNEL_MEMORY with #if (1) and #endif.
Regards,
David
I have already install the MQX plugin, I am not sure how I can remove it and then re add it. I don't know how to remove a plugin in eclipse.
In MQX1.c kernel_data_prv is undeclared, so I get an error. But _mqx_kernel_data_struct is i think the same thing, so i made the substitution for __KERNEL_DATA_START.
/* START OF KERNEL MEMORY */ &_mqx_kernel_data_struct,
/* END OF KERNEL MEMORY */ (pointer)((uchar_ptr)&_mqx_kernel_data_struct + sizeof(_mqx_kernel_data_struct)),
No change.
At my work computer it seems that things are working better. MQX now loads the run time kernel data, with the exception of the Kernel Log (I will look into this).
But my call stack still only shows the stack for the active task. Any way to get the same functionality of CW???
NVM!!!
Recompiled and MQX views are no longer syncing with my MQX runstate, so this seems to be an intermitant problem ?
Leif
hello Leif,
from my understanding, TAD must work with MQX plugin installed. please refer this thread to install it:
Problem: Installing MQX RTOS Task Aware Debugger for GDB plug-in (TAD)
can it help?
Have a great day,
Zhang Jun
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
MQX plug-ins are installed. I see the MQX menu with all the debugging views, just no valid data.
That post seems to deal with installation problems, I don't believe I have an installation problem.
Unless I am missing something?