Hi Freescalers,
Is the K22 supported by CodeWarrior + MQX 4.2 ?
The document MQX Roadmap says :
MQX RTOS 4.2 (Released May 5, 2015)
MCUs Supported
General Updates
- I found errors in UART part (BSP) : K22FN512 and MQX UART (MUX and baudrate)
- No support for USB part : with the BSP Cloning tool, the USB lib is not generated (even not present in the Freescale_MQX_4_2\usb\host\build\cw10gcc directory).
So, is there a way to use this whole chip with MQX4.2 + CW ?
Yvan
PS : don't tell me about KDS...
解決済! 解決策の投稿を見る。
Hi Yvan
Thank you for your feedback. I know your feelings.
I have discussed your question with my colleague. Unfortunately, there is no MQX BSP support for K22 in Codewarrior 10.6. Now Freescale’s software strategy going forward is based on the Kinetis SDK. The supported IDE includes IAR,Keil , KDS and Atollic. But no Codewarrior. It means in the future, we will not integrate new features into Codewarrior. I don't think you can use k22 with codewarrior and MQX. there are lots of work to do. Though you don't like KDS, in fact, KDS is a replacement of Codewarrior for the new Kinetis devices. They are very similar. and it is free. If you wants to have a try, I suggest you use KDS 3.0. there is a user guide in your installation folder. C:\Freescale\KDS_3.0.0\doc.
Of course you can choose IAR or Keil.
Regards
Daniel
Hi Yvan
Thank you for your feedback. I know your feelings.
I have discussed your question with my colleague. Unfortunately, there is no MQX BSP support for K22 in Codewarrior 10.6. Now Freescale’s software strategy going forward is based on the Kinetis SDK. The supported IDE includes IAR,Keil , KDS and Atollic. But no Codewarrior. It means in the future, we will not integrate new features into Codewarrior. I don't think you can use k22 with codewarrior and MQX. there are lots of work to do. Though you don't like KDS, in fact, KDS is a replacement of Codewarrior for the new Kinetis devices. They are very similar. and it is free. If you wants to have a try, I suggest you use KDS 3.0. there is a user guide in your installation folder. C:\Freescale\KDS_3.0.0\doc.
Of course you can choose IAR or Keil.
Regards
Daniel
Daniel,
Thanks for your answer.
To resume, I need an OS (MQX) and I already tried KDS 3.0.0 + KDSK 1.2.0, but it's so very different and so hard to use than CW + MQX...
Free or not is not the problem for me, I just need an usable and friendly IDE.
With KDS, FREESCALE has now no solution for me ; I'm trying another solution for this middle range of CPU : TI MSP430 and their CSS+TI_RTOS.
My future devs with "big" M4 will be with K64 + CW + MQX. But the day when all CPU's will be on KDS, I'll have to change this solution too.
Yvan