MQX 4.2 IMX6SX BSP Missing?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MQX 4.2 IMX6SX BSP Missing?

ソリューションへジャンプ
1,077件の閲覧回数
w2vy
Contributor V

macl

As shown on the page announcing the 4.2 release, there was a 4.1 patch that provided support for the i.MX6 SoloX M4 core.

I downloaded the 4.2 release and did not see the SoloX BSP.

Was that an oversight?

Tom

0 件の賞賛
返信
1 解決策
831件の閲覧回数
macl
Senior Contributor I

Hi,

No oversight.  The I.MX 6 SoloX BSP is provided in the separate MQX 4.1-based standalone release.  Architecturally it is a bit different and was better kept in its own branch.  To my knowledge, the updates in MQX 4.2 aren't applicable for the SoloX BSP since it does not include TCP/IP or file system.   Hope this helps.

Thanks,

Mac

元の投稿で解決策を見る

0 件の賞賛
返信
3 返答(返信)
832件の閲覧回数
macl
Senior Contributor I

Hi,

No oversight.  The I.MX 6 SoloX BSP is provided in the separate MQX 4.1-based standalone release.  Architecturally it is a bit different and was better kept in its own branch.  To my knowledge, the updates in MQX 4.2 aren't applicable for the SoloX BSP since it does not include TCP/IP or file system.   Hope this helps.

Thanks,

Mac

0 件の賞賛
返信
831件の閲覧回数
w2vy
Contributor V

Ok thanks, that makes sense. from the naming I thought the release was a PATCH to 4.1, but upon looking closer it is a stand alone release

thanks!

See you at FTF!

0 件の賞賛
返信
831件の閲覧回数
johannesstuttne
Contributor II

Hi, is their any TCP/IP support planed in the mqx version for the imx6SX?

0 件の賞賛
返信