Hi,
(CW10.5, MQX4.0.2)
I cloned the BSP TWR-K60N512 for my project that use a MK60DN512VLQ10.
In the BSP tower project it is a MK60DN512Z (define PSP_CPU_MK60DN512Z). I tried to change in PE the processor type (add new and disable the Z) and I have some issues in MQX files. (I2S mainly)
Can someone help me to understand why a uC that should not be used for new design (the Z) is supported in MQX and not the current one?
Or maybe I am missing something but at this point I loose my minds. (I checked the reference manual and I can see the difference in the IO_Map.h correspond to the differences in the manual)
I will try now the clone a BSP from the twr-k60d100m now to see the difference.
Thanks
BR
stéphan
Solved! Go to Solution.
At this point I succeeded by starting from the TWR-K60D100M that is the correct family. I can see that the BSP files and all io files are related to the non-"Z" version now. :-)
At this point I succeeded by starting from the TWR-K60D100M that is the correct family. I can see that the BSP files and all io files are related to the non-"Z" version now. :-)