I am trying to use the i2s_demo code on a K70 board and MQX 4.1. It's all going well until the first write() to the sai1: device. In the "play" shell command there is this loop:
/* Play a file */ printf(" Playing a file..."); while (!feof(file_ptr)) { requested = fread(data, 1, block_size, file_ptr); if (ferror(file_ptr) && !(feof(file_ptr))) { printf("\n Error reading from a file %s.\n", argv[2]); break; } write(device_ptr, data, requested); }
Line 13 above is going to end up calling _io_sai_int_write() below:
_mqx_int _io_sai_int_write ( /* [IN] the handle returned from _fopen */ MQX_FILE_PTR fd_ptr,
/* [IN] where the data are to be stored */ char *data_ptr,
/* [IN] the number of bytes to read */ _mqx_int n ) { /* Body */ IO_DEVICE_STRUCT_PTR io_dev_ptr; IO_SAI_DEVICE_STRUCT_PTR io_sai_dev_ptr; uint32_t result;
io_dev_ptr = (IO_DEVICE_STRUCT_PTR)fd_ptr->DEV_PTR; io_sai_dev_ptr = (void *)io_dev_ptr->DRIVER_INIT_PTR; _lwsem_wait(&io_sai_dev_ptr->LWSEM);
result = (*io_sai_dev_ptr->DEV_WRITE)(io_sai_dev_ptr, data_ptr, n); _lwsem_post(&io_sai_dev_ptr->LWSEM); return result;
} /* Endbody */
In line 22 in _io_sai_int_write() above, (*io_sai_dev_ptr->DEV_WRITE) is 0x00000000 !!
That's because in init_sai.c in the BSP the read and write function pointers are set to NULL:
const SAI_INIT_STRUCT _bsp_sai_init = { "sai1:", _ksai_dma_init, _ksai_dma_deinit, NULL, NULL, _ksai_dma_ioctl, &_bsp_ksai_init };
What's going on with this demo?
Paul
已解决! 转到解答。