I have a TWR-K20D50M board, USB Host documentation is wrong!

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

I have a TWR-K20D50M board, USB Host documentation is wrong!

753件の閲覧回数
GenkiKai
Contributor I

In the MQX documentation for the TWR-K20D50M board it states "For using USB Host mode, jumpers on position: TWR-K20D50M board, J26 on position 1-2 (That's correct), TWR-K20D50M board, J30 on position 5-6 (VREGIN)."  This last jumper J30 5-6 IS INCORRECT.  That position, when the TWR board is hooked up to a USB Device (like a mouse) leaves the MCU UNPOWERED.  J30 5-6 powers the MCU from the micro USB port.  A USB Device has no power!  When connected to a PC having J30 on position 1-2 powers the MCU with 1.8 volts.When connected to a PC having J30 on position 5-6 powers the PC with anywhere from 5.2 to 6.5 volts (PC USB Powered).

0 件の賞賛
返信
3 返答(返信)

576件の閲覧回数
GenkiKai
Contributor I

HI Daniel,

Take a look at the schematic again.  Then inputs to J30 are "(6) P5V_K20_USB" for Jumper position 5 and "P5V_TRG_USB" for Jumper poistion 1.  When the board is hooked up to a standard USB device, like a mouse, the is no USB power!  A USB device cannon SUPPLY power, so using Jumper position 5 leaves the MCU UNPOWERED. With an USB device that cannot supply power you HAVE to use Jumper position 1 to get power to the MCU.

0 件の賞賛
返信

576件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Alan:

I tested the host  hid_mouse demo with the TWR-K20D50M board.

C:\Freescale\Freescale_MQX_4_2\usb\host\examples\hid\mouse

When Jumper 30 position 1-2, this demo can work, but VREGIN is 2.1v,  not meets the USB spec. Maybe some other demos can't work.

When Jumper 30 position 5-6,  MCU unpowered.

When Jumper 30 position 5-6 and together with default setting 1-2 , then VREGIN is 5V, meets the USB spec. So for using host mode, jumper 30 should be position on 5-6 , and 1-2.

This documentation seems not very clear. I will inform the document team about this.

Thanks for your feedback.

Regards

Daniel

0 件の賞賛
返信

576件の閲覧回数
danielchen
NXP TechSupport
NXP TechSupport

Hi Alan:

J30 should be on position 5-6 for  using USB host mode, also for using USB device mode.

Please see the below picture.

usb-host-power.jpg

usb-host-2.jpg

For Host mode, J26 is position 1-2,  P5V_USB powers Micro USB port and VREGIN.

For Device mode, J26 is open,  Micor USB port powers VREGIN

Regards

Daniel

0 件の賞賛
返信