I'm using FNET bootloader and MQX with RTCS on K60 tower and ethernet works fine.
I need to change PHY device (ksz8041nl on tower board) to switch device (KSZ8863RLL) so it means change MAC(K60)<->PHY to MAC(K60)<->MAC connection, I think.
I wonder if is it difficult to change firmware of FNET and RTCS to work properly with this hardware change?
解決済! 解決策の投稿を見る。
I am using both KSZ8041 and KSZ8873 and they both work with the same firmware.
I am using a MCF52259 and I modified the BSP by using the DEMO board example on the EVB platform.
There is no files for the KSZ8873 but it is very similar to the KSZ8041 so it works.
In the future I would like to add the additional features of the switch.
I am using both KSZ8041 and KSZ8873 and they both work with the same firmware.
I am using a MCF52259 and I modified the BSP by using the DEMO board example on the EVB platform.
There is no files for the KSZ8873 but it is very similar to the KSZ8041 so it works.
In the future I would like to add the additional features of the switch.