Hi Everyone,
We are interfacing K70 with LPDDR (MT46H32M16LF – 8 Meg x 16 x 4 banks) and facing issues with our current configuration. Please let us know if there is any error in our configuration. Also it would be helpful if some one could provide us the correct LPDDR configuration.
Our configuration is as follows,
int ddr_init_script(void)
{
if ((SIM_SCGC3 & SIM_SCGC3_DDR_MASK) != SIM_SCGC3_DDR_MASK)
{
// Enable DDR clock gate
SIM_SCGC3 |= SIM_SCGC3_DDR_MASK;
}
else
{
// Check to if the DRAMC is already initialized
if ((DDR_CR00 & 1) == 1)
return 1;
}
// Setup drive strength & enable IO pad
SIM_MCR &= 0xFFFFFF00;
SIM_MCR |= 0x00000004;
// Setup IO pad ODT, 700mV seperation & spare dly ctrl
#define DDR_PAD_CTRL *((volatile unsigned long*)0x400AE1AC)
DDR_PAD_CTRL = 0x00030203;
SIM_MCR |= 0x100; // DDR RCR reset
SIM_MCR &= ~0x100; // DDR RCR out of reset
DDR_CR00 = 0x00000100; // DDRCLS, start
DDR_CR02 = 0x00007530; // initaref, tinit
DDR_CR03 = 0x01010707; // tccd, wrlat, latgate, latlin
DDR_CR04 = 0x07090201; // trasmin, trc, trrd, tbint
DDR_CR05 = 0x02000302; // tmrd, trtp, trp, twtr
DDR_CR06 = 0x01290404; // intwbr, trasmax, tmod
DDR_CR07 = 0x01010202; // ccapen, ap, tckesr, clkpw
DDR_CR08 = 0x06030300; // tdal, twr, trasdi, tras
DDR_CR09 = 0x020000c8; // bstlen, nocmd, tdll
DDR_CR10 = 0x03000002; // trpab, tcpd, tfaw
DDR_CR11 = 0x01000000; // trefen, arefmode, aref, regdimm
DDR_CR12 = 0x048a000b; // tref, trfc
DDR_CR13 = 0x00000005; // pd, trefint
DDR_CR14 = 0x00110002; // txsr, tpdex
DDR_CR15 = 0x0000000b; // puref, sref, txsnr
DDR_CR16 = 0x00000001; // lpctrl, clkdly, qkref
DDR_CR20 = 0x00030300; // cksrx, cksre, lpre
DDR_CR21 = 0x00000032; // mr1dat0, mr0dat0
DDR_CR25 = 0x0a010300; // aprebit, colsiz, addpins, bnk8
DDR_CR26 = 0x0101ffff; // bnkspt, addcol, cmdage, agecnt
DDR_CR27 = 0x00010101; // swpen, rwen, prien, plen
DDR_CR28 = 0x00000001; // cmdlatr, bigend, reduc, csmap
DDR_CR30 = 0x00000001; // intack, rsyncrf
DDR_CR34 = 0x00000101; // odtwrcs, odtrdcs
DDR_CR37 = 0x00000200; // w2wsame, w2rsame, r2wsame, r2rsame
DDR_CR38 = 0x00200000; // p0wrcnt, pupcs, pdncs
DDR_CR39 = 0x00000020; // wp0, rp0, p0rdcnt
DDR_CR40 = 0x00002000; // p1wrcnt, p0typ
DDR_CR41 = 0x01010020; // wp1, rp1, p1rdcnt
DDR_CR42 = 0x00002000; // p2wrcnt, p1typ
DDR_CR43 = 0x02020020; // wp2, rp2, p2rdcnt
DDR_CR45 = 0x00070b0f; // p0pri3, p0pri2, p0pri1, p0pri0
DDR_CR46 = 0x0f004000; // p1pri0, p0prirlx, p0ord
DDR_CR47 = 0x0100070b; // p1ord, p1pri3, p1pri2, p1pri1
DDR_CR48 = 0x0b0f0040; // p2pri1, p2pri0, p1prirlx
DDR_CR49 = 0x00020007; // p2ord, p2pri3, p2pri2
DDR_CR50 = 0x00000040; // p2prirlx
DDR_CR52 = 0x02000602; // rddtenbas, phyrdlat, phywrltbs
DDR_CR56 = 0x01030000; // wrlatadj, rdlatadj
DDR_CR57 = 0x01000000; // odtalten
DDR_CR00 |= 1; // DDRCLS, start
while ((DDR_CR30 & 0x400) != 0x400);
// Setup memory address translation
MCM_CR |= MCM_CR_DDRSIZE(0);
return 1;
}
We created this configuration using this https://www.freescale.com/webapp/Download?colCode=KINETIS_K70_DDR_INIT&location=null&Parent_nodeId=&... tool.
Thanks
Pramod
解決済! 解決策の投稿を見る。
Hi,
The MQX BSP function that initializes SDRAM controller can be found in the source file
c:\Freescale\Freescale_MQX_4_x\mqx\source\bsp\twrk70f120m\init_hw.c.
_bsp_ddr2_setup
called by init_hardware() in the same file.
I attached the init for the mt46h32m16lf part. I hope this helps!!!!
Freescale also provides below application note about DDR2 SDRAM hardware design and initialization:
AN2910 (Hardware and Layout Design Considerations for DDR2 SDRAM Memory Interfaces) :
http://cache.freescale.com/files/32bit/doc/app_note/AN2910.pdf
AN3522 (DDR2 SDRAM on the ColdFire MCF5545x Microprocessor) : http://cache.freescale.com/files/32bit/doc/app_note/AN3522.pdf
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi,
The MQX BSP function that initializes SDRAM controller can be found in the source file
c:\Freescale\Freescale_MQX_4_x\mqx\source\bsp\twrk70f120m\init_hw.c.
_bsp_ddr2_setup
called by init_hardware() in the same file.
I attached the init for the mt46h32m16lf part. I hope this helps!!!!
Freescale also provides below application note about DDR2 SDRAM hardware design and initialization:
AN2910 (Hardware and Layout Design Considerations for DDR2 SDRAM Memory Interfaces) :
http://cache.freescale.com/files/32bit/doc/app_note/AN2910.pdf
AN3522 (DDR2 SDRAM on the ColdFire MCF5545x Microprocessor) : http://cache.freescale.com/files/32bit/doc/app_note/AN3522.pdf
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------