This sub question is also buried in another thread but so I wanted to ask this as an explicit new question.
I have set the bsp user_config.h file for "ittya:" and as the BSP_DEFAULT_IO_CHANNEL but I need PTA14 ALT3 on the K40dx256 to use UART0 TX0. How do I go about doing that in mqx? I know how to do this outside of mqx using Device Init but I don't see how to select a specific pin within an specific ALT configuration within MQX.
Right now I have mqx running correctly and opening the file block for the UART and using a printf but nothing comes out on the pin. Hence my assumption that the internal configuration is not correct.
Can anyone point me in the right direction please? Thanks
Robert
解決済! 解決策の投稿を見る。
IDE: CW10.3
MQX: 4.0
MCU: K60
Here is my experience for K60
modify _bsp_serial_io_init()
navigation to init_gpio.c
in CodeWarrior Projects window
bsp_twrk60d100m -> twrk60d100m BSP Files -> init_gpio.c
function
/*FUNCTION*-------------------------------------------------------------------
*
* Function Name : _bsp_serial_io_init
* Returned Value : MQX_OK for success, -1 for failure
* Comments :
* This function performs BSP-specific initialization related to serial
*
*END*----------------------------------------------------------------------*/
_mqx_int __bsp_serial_io_init()
here is the setting of AUX for UART0 (for K60)
case 0:
pctl = (PORT_MemMapPtr)PORTD_BASE_PTR;
if (flags & IO_PERIPHERAL_PIN_MUX_ENABLE)
{
/* PTD6 as RX function (Alt.3) + drive strength */
pctl->PCR[6] = 0 | PORT_PCR_MUX(3) | PORT_PCR_DSE_MASK;
/* PTD7 as TX function (Alt.3) + drive strength */
pctl->PCR[7] = 0 | PORT_PCR_MUX(3) | PORT_PCR_DSE_MASK;
}
I think it is the same source code file/function for K40
Leslie
IDE: CW10.3
MQX: 4.0
MCU: K60
Here is my experience for K60
modify _bsp_serial_io_init()
navigation to init_gpio.c
in CodeWarrior Projects window
bsp_twrk60d100m -> twrk60d100m BSP Files -> init_gpio.c
function
/*FUNCTION*-------------------------------------------------------------------
*
* Function Name : _bsp_serial_io_init
* Returned Value : MQX_OK for success, -1 for failure
* Comments :
* This function performs BSP-specific initialization related to serial
*
*END*----------------------------------------------------------------------*/
_mqx_int __bsp_serial_io_init()
here is the setting of AUX for UART0 (for K60)
case 0:
pctl = (PORT_MemMapPtr)PORTD_BASE_PTR;
if (flags & IO_PERIPHERAL_PIN_MUX_ENABLE)
{
/* PTD6 as RX function (Alt.3) + drive strength */
pctl->PCR[6] = 0 | PORT_PCR_MUX(3) | PORT_PCR_DSE_MASK;
/* PTD7 as TX function (Alt.3) + drive strength */
pctl->PCR[7] = 0 | PORT_PCR_MUX(3) | PORT_PCR_DSE_MASK;
}
I think it is the same source code file/function for K40
Leslie
Hi Leslie
What you have suggested makes sense; I could not find any port/bit.uart spcific info on setup. I will give it a try.
Thank you very much for the answer.
Robert
Hi Leslie
That was it; works perfectly. Thanks again
Robert