sbc_fs65 generator fail

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

sbc_fs65 generator fail

Jump to solution
869 Views
TerryDuPower
Contributor III

Dear supporter:

     I careated a project with SDK.  Add a component sbc_fs65, But it failed to generate code.

TerryDuPower_0-1652166826988.png

Component: sbc_fs651 of type sbc_fs65<br/>Description: S32 SDK Middleware for System Basis Chip FS65 family<br/><i>Repository: SDK_S32_PA_10</i>

0 Kudos
Reply
1 Solution
828 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

I was able to reproduce it in RTM 3.0.0. It was obviously fixed in 3.0.3, so my recommendation is to install the latest update and use 3.0.3:

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-Power-Architectu...

Regards,

Lukas

View solution in original post

3 Replies
839 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

which SDK version you have? I did quick test in latest version 3.0.3. I created new project for MPC5775B, added sbc_fs65 component, it asked me to add also referenced dma and osif components. Then I added init function of SBC and I can generate the code and compile the project.

Regards,

Lukas

0 Kudos
Reply
835 Views
TerryDuPower
Contributor III

Hi lukaszadrapa,

   I used the SDK version 3.0.0.

TerryDuPower_0-1652405254574.png

Thanks!

Regards!

0 Kudos
Reply
829 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

I was able to reproduce it in RTM 3.0.0. It was obviously fixed in 3.0.3, so my recommendation is to install the latest update and use 3.0.3:

https://community.nxp.com/t5/S32-Design-Studio-Knowledge-Base/S32-Design-Studio-for-Power-Architectu...

Regards,

Lukas