Hello
I am going to compile the MPC574XP_MCAL4_0_RTM_2_0_2 example with the makefile by launching launch.bat , but I got an error:
make (e=2) : the system cannot find the file specified.
make.exe: *** [Adc.o] Error 2
Could anybody help?
解決済! 解決策の投稿を見る。
Hello @Ehsaaan ,
Could you please check if you have filled the correct value for the MAKE_DIR, TRESOS_DIR, ... in the launch.bat file. Eg:
Best regards,
Hung
Hello @Ehsaaan ,
Have you resolved the configuration issue. If not could you please share your EB project or at least the Mcu configuration(.xdm or .epc). Then I will check it.
Best regards,
Hung
You should try with the compiler version mentioned in the Release note:
The newer version might update some features which MCAL were not verified with.
Best Regards,
Nam
Hello @Ehsaaan ,
Could you please check if you have filled the correct value for the MAKE_DIR, TRESOS_DIR, ... in the launch.bat file. Eg:
Best regards,
Hung
Hello.
@hungnguyenphi
Yes, that problem is solved now, I set the compiler direction wrong.
But now I have some new problems...
the error log and other info are attached here.
Hello @Ehsaaan ,
Could you please share your EB project of the Mcu configuration file(.xdm or .epc file).Then I will check it.
Best regards,
Hung