Hi, I am using mpc #5674f and I have to work with #uart peripheral in it. If I successfully initiate uart and be able to receive data with it, but failed to transmit any bytes.
I am using the project atteched below. This is an example, and the link :Example XPC567XFKIT PinToggleStationery CW210
Can anyone help me?
Thank you in advance.
Regards.
已解决! 转到解答。
Thanks a lot! I got it!
1. And could you please send me a flexcan example of mpc5674f,.
Now I got one, but it doesn't work. The following is the example I downloaded from the Community,
2. And also, when I generated C code of 5674f using RAppID ,and compiled, a error arised, it said cannot open prefix file vle_macro.txt.
In the settings, I added the vle_macro.txt as the "Using-RAppID-with-codewarror.pdf" requested.
Regards
Jason Su
Thanks a lot! I got it!
1. And could you please send me a flexcan example of mpc5674f,.
Now I got one, but it doesn't work. The following is the example I downloaded from the Community,
2. And also, when I generated C code of 5674f using RAppID ,and compiled, a error arised, it said cannot open prefix file vle_macro.txt.
In the settings, I added the vle_macro.txt as the "Using-RAppID-with-codewarror.pdf" requested.
Regards
Jason Su