What is the meaning of “PARTITION” in MPC5645S

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

What is the meaning of “PARTITION” in MPC5645S

ソリューションへジャンプ
1,490件の閲覧回数
hyacinth
Contributor II

Dear All,

In the description of Flash for MPC5645S,L0 to L3 are located in Patition 1,L4 to L7 are located in Patition 2...

When erase the Blocks,is there anything special within a patition?And What is the physical Meaning of  Patition here?

pastedImage_1.png

BR

Chen

ラベル(1)
1 解決策
1,012件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, code may be executed from one partition while another one is being programmed. That's the reason for flash partitions.

元の投稿で解決策を見る

4 返答(返信)
1,013件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, code may be executed from one partition while another one is being programmed. That's the reason for flash partitions.

1,012件の閲覧回数
hyacinth
Contributor II

So,when the code is executed from L1 and L2, it is not allowed to program L3?

0 件の賞賛
返信
1,012件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

You are right.

1,012件の閲覧回数
hyacinth
Contributor II

Thanks for your reply, it's sloved the problem perfectly!

0 件の賞賛
返信