Dear All,
In the description of Flash for MPC5645S,L0 to L3 are located in Patition 1,L4 to L7 are located in Patition 2...
When erase the Blocks,is there anything special within a patition?And What is the physical Meaning of Patition here?
BR
Chen
已解决! 转到解答。
Hi, code may be executed from one partition while another one is being programmed. That's the reason for flash partitions.
在原帖中查看解决方案
So,when the code is executed from L1 and L2, it is not allowed to program L3?
You are right.
Thanks for your reply, it's sloved the problem perfectly!