The stop mode of MPC5606S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The stop mode of MPC5606S

746 Views
松王
Contributor I

Hello ,everybody

    I am using the MPC5606S-DEMO-V2 board for my test, The version of schematic is SCH-26640 REV C ,The example project I used is from Freescale too.the consumption can't go down to which is described on the manual.(1.8mA max  of 25℃).Can anybody share the code which can reach 1.8mA  on the demo board?

    thanks!

Wilson

Labels (1)
0 Kudos
Reply
1 Reply

603 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello Wilson,

On which pins you are measuring the current consumption? Remember to measure the current as close to micro as possible.

Unfortunately there is not available an example you have requested.

Have a look at application note dealing with low power modes:

http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4240.pdf

0 Kudos
Reply