Hello ,everybody
I am using the MPC5606S-DEMO-V2 board for my test, The version of schematic is SCH-26640 REV C ,The example project I used is from Freescale too.the consumption can't go down to which is described on the manual.(1.8mA max of 25℃).Can anybody share the code which can reach 1.8mA on the demo board?
thanks!
Wilson
Hello Wilson,
On which pins you are measuring the current consumption? Remember to measure the current as close to micro as possible.
Unfortunately there is not available an example you have requested.
Have a look at application note dealing with low power modes:
http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4240.pdf