HI
My SJA1105T can`t work normal,i need some help.
I had detect signals at TXD[0:3] from MCU to SWITCH, but i can`t detect signals at TXD[0:3] from SWITCH to PHY.
I had get some information from Software user manual for SJA1105TEL .
I read the Initial device configuration flag register ,it shows the configuration is valid.
I read the Ethernet high-level port status diagnostic counters part 1 ,the N_RXFRM \N_RXFRMSH \N_TXFRM\ N_TXFRMSH which show the tx/rx frames counter is always 0.
why?
已解决! 转到解答。
If N_RXFRM doesn't change when you send traffic to the corresponding
port, it means the port is unable to detect a proper frame. This in
turn may happen due to wrong timing of the MII interface signals or
because the port is improperly or not fully configured. Suggestions:
1. Check error counters and flags described in UM10944, Section 5.1.4.1
2. Make sure CGU and ACU are properly configured for the used interface
type. Note that this configuration is not part of the static configuration
sequence. See AH1601 for more details, the document is available
on Docstore.
Have a great day,
Platon
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
If N_RXFRM doesn't change when you send traffic to the corresponding
port, it means the port is unable to detect a proper frame. This in
turn may happen due to wrong timing of the MII interface signals or
because the port is improperly or not fully configured. Suggestions:
1. Check error counters and flags described in UM10944, Section 5.1.4.1
2. Make sure CGU and ACU are properly configured for the used interface
type. Note that this configuration is not part of the static configuration
sequence. See AH1601 for more details, the document is available
on Docstore.
Have a great day,
Platon
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
and the Ethernet port status - diagnostic flags is all 0, I don`t know what this means.
2.The static configuration sequence, I get from simpleT.py, and It's been modified a little bit to match my board
//MII CLOCK FOR PORT0 (PHY)
static const uint8_t port0_idiv0[] = {0x01|0x80,0x00,0x00,0xb0,0x0a,0x00,0x00,0x00};
static const uint8_t port0_mii_tx_clk[] = {0x01|0x80,0x00,0x01,0x30,0x11,0x00,0x08,0x00};
static const uint8_t port0_mii_rx_clk[] = {0x01|0x80,0x00,0x01,0x40,0x01,0x00,0x08,0x00};
static const uint8_t port0_ext_tx_clk[] = {0x01|0x80,0x00,0x01,0x80,0x11,0x00,0x08,0x00};
static const uint8_t port0_ext_rx_clk[] = {0x01|0x80,0x00,0x01,0x90,0x11,0x00,0x08,0x00};
//MII CLOCK FOR PORT1 (MAC)
static const uint8_t port1_idiv1[] = {0x01|0x80,0x00,0x00,0xc0,0x0a,0x00,0x00,0x01};
static const uint8_t port1_mii_tx_clk[] = {0x01|0x80,0x00,0x01,0xa0,0x02,0x00,0x08,0x00};
static const uint8_t port1_mii_rx_clk[] = {0x01|0x80,0x00,0x01,0xb0,0x03,0x00,0x08,0x00};
//MII CLOCK FOR PORT2 (MAC)
static const uint8_t port2_idiv2[] = {0x01|0x80,0x00,0x00,0xd0,0x0a,0x00,0x00,0x01};
static const uint8_t port2_mii_tx_clk[] = {0x01|0x80,0x00,0x02,0x10,0x04,0x00,0x08,0x00};
static const uint8_t port2_mii_rx_clk[] = {0x01|0x80,0x00,0x02,0x20,0x05,0x00,0x08,0x00};
//MII CLOCK FOR PORT0 (MAC)
static const uint8_t port3_idiv3[] = {0x01|0x80,0x00,0x00,0xe0,0x0a,0x00,0x00,0x01};
static const uint8_t port3_mii_tx_clk[] = {0x01|0x80,0x00,0x02,0x80,0x06,0x00,0x08,0x00};
static const uint8_t port3_mii_rx_clk[] = {0x01|0x80,0x00,0x02,0x90,0x07,0x00,0x08,0x00};
//MII CLOCK FOR PORT0 (MAC)
static const uint8_t port4_idiv4[] = {0x01|0x80,0x00,0x00,0xf0,0x0a,0x00,0x00,0x01};
static const uint8_t port4_mii_tx_clk[] = {0x01|0x80,0x00,0x02,0xf0,0x08,0x00,0x08,0x00};
static const uint8_t port4_mii_rx_clk[] = {0x01|0x80,0x00,0x03,0x00,0x09,0x00,0x08,0x00};
4.The ACU part
/* Configure CFG_PAD_MII0_RX[CLK_IPUD], Pull down MII0_RX_ER */
static uint8_t tmp[8] = {0x01|0x80,0x00,0x80,0x10,0x02,0x02,0x03,0x12};
If you find any problems,i will really appreciate.