TSENS0 and TSENS1 comparison

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TSENS0 and TSENS1 comparison

755 Views
apu_apustaja
Contributor II

Hello, we're defining and implementing safety requirements in our system based on MPC5744P, while referring to the MPC5744P Safety Manual.

In it, the SM_066 quotes:

During power up, the two temperature sensors are to be read by
software (TSENS0 from ADC0 channel 15, TSENS1 from ADC1 channel 15). The
software must verify that the conversion values are similar, as this is a means of assessing
that the sensors are working properly. [end]

Is there a recommendation as for what does "similar" mean? Is there any information for what would be the theoretical maximum allowed difference between the two?

Thanks, and best regards

0 Kudos
Reply
2 Replies

734 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi,

as accuracy of temperature sensor is defined as +/- 3%, 'similar' could be defined as difference up to 6%

0 Kudos
Reply

649 Views
apu_apustaja
Contributor II

Thanks for the response, could you please just clarify if these sensors are on the exact same physical location on the chip, where actual temperature differences would therefore be not very likely?

Or are they on separate locations, and actual temperature difference should be taken into consideration, and then the tolerable difference would be above 6%?

Because in our testing, the difference often shows >6%.

0 Kudos
Reply