I need to use SPI to communicate with EEPROM, SPC5746R as the Master to send and receive, the timing of EEPROM is as follows:
However, after I finish sending data using "SPI_MasterTransferBlocking" in SDK, the Master does not provide the clock signal for the slave to transfer data back. How should I operate and set up to correctly read the data returned by the EEPROM?
Did I call the read function wrong?
Solved! Go to Solution.
Hi,
send 2 bytes using SPI_MasterTransferBlocking function, first byte is instruction, second is dummy byte.
BR, Petr
Hi,
send 2 bytes using SPI_MasterTransferBlocking function, first byte is instruction, second is dummy byte.
BR, Petr