We can set the number of sample(256,I set)in a chirp in the SPT module, and then we can set the number of chirp(128,I set) in a frame. This means that when SPT.GBL_STATUS.B.FRM_ACQ_DONE is set, we should adopt 256*128 data, but only the actual 128*208 data, if I increase the value of sample, the effective numerical maximum of only 208.
What's even more puzzling is that I reduce the value of sample, the number of actual sampling points will also be reduced, not the value of sample I set, of course, the actual value has been a multiple of 8.
What's wrong with this? How do I fix it?
Hi,
ADAS peripherals are very specific and they are supported only on request.
Therefore I do not expect someone here on community will answer to your query.
If you wan to get in touch with experts you have to submit a ticket:
Peter
Hi,
I'm sorry to tell you that I tried to submit case, but didn't give me any help.