SDADC of MPC5775K

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDADC of MPC5775K

2,043 Views
wangbin
Contributor II

Hi,

I want to power up all SDADC's simultaneously,but the last channel has no data,the data of the other 7 channels are correct.Please tell me how to configure SDADC.

Thanks!

9 Replies

1,495 Views
yijunzheng
Contributor I

I met the same problem about SDADC. The value of 0~6 channels of SDADC is correct, but the value in last channel is almost 0. I checked the state of SDADC channel, it seems the Channel H is always keep in over voltage and over load status.

ADCOVLD.JPG

I try to disable over voltage protection via clear ADCCTRL7_OVPWRDN. But this switch bit seems only have effect to channel 0-6. Channel 7 still in over voltage status when I have closed the over voltage protection.

ADCCTRL7.JPG

@Peter Vlna 员工  Are there any expert can give me some idea about this feature.

0 Kudos
Reply

1,495 Views
eleclin
Contributor II

Hello

I am working on SDADC of MPC5775K too. I configured the register as reference manual recommended. But I can not see any data in SRAM using SDMA when the SDMA address was 0x40000000 and  FRM__ACQ_DONE flag was set correctly. Could you give me some help or any example about SDADC with SDMA configuration.

Regards

Hai

0 Kudos
Reply

1,495 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I am not so familiar with radar modules, but I will try to explain the situation.

You have acquired data via SDADC correctly. So you can see conversion is ended.

I expect that on end of conversion is DMA transfer triggered.

You have to correctly configure DMA to HW trigger request from SDADC.

I also expect that you must configure AIPS so the master (DMA) can access slaves.

If you done all this configuration correctly I see no other issues here and data transfer should work as required.

Peter

1,495 Views
wangbin
Contributor II

Who can help me?

0 Kudos
Reply

1,495 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The radar modules are supported only on request as the applications are very customer specific.

I do not expect that someone outside NXP will help you with this topic on community.

We have posted one simple example on SDADC here:

https://community.nxp.com/docs/DOC-330909 

We will most probably create a set of some general examples for external use in future.

Peter

1,495 Views
junyishen
Contributor II

I want to configure SDADC,too.But there is no example .You say that the data of the other 7 channels are correct.where is the data stored??what is the address?

0 Kudos
Reply

1,495 Views
wangbin
Contributor II

You may try to configure SDMA to specify an address.

0 Kudos
Reply

1,495 Views
junyishen
Contributor II

I've been able to sample data and read data from SDMA, but I have another problem.

We can set the number of sample(256,I set)in a chirp in the SPT module, and then we can set the number of chirp(128,I set) in a frame. This means that when SPT.GBL_STATUS.B.FRM_ACQ_DONE is set, we should adopt 256*128 data,  but only the actual 128*208 data, if I increase the value of sample, the effective numerical maximum of only 208.

Have you ever had this problem?Or maybe the last channel didn't have all 0 data, but it was missing data like me.

0 Kudos
Reply

1,495 Views
junyishen
Contributor II

Hi

CTE triggers ADC sample capture.But I don't know how to configure CTE .Could you give me any example or your code?

regards

Junyi

0 Kudos
Reply