S32DS failed to download program into MPC5748G due to misoperation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS failed to download program into MPC5748G due to misoperation

747 Views
mahoneinsh
Contributor I

Dear NXP supporter:
Development enviroment of the project is:S32DS_Power_v2017.R1, PE multilink universal, MPC5748G

I have encountered a serious problem because of my misoperation. The power of my mpc5748g board turned off  when i was downloading program with PE multilink universal. Then i restarted the power and downloaded program again, it still failed. The download progress was stucked shown as followed.

mahoneinsh_0-1678451891667.png

I have tried many times to download, but the boad still can not work, it seems like the chip was damage.

Could you tell me why turning off power when downloading program would result in this problem? and, how can i solve this problem?

Thank you in advance~

 

 

 

0 Kudos
Reply
3 Replies

734 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it's caused by watchdog and reset escalation, most likely. Take a look at this post:

https://community.nxp.com/t5/MPC5xxx/MPC5748G-is-always-in-reset/m-p/1222737/highlight/true#M17232

In the same thread, there's also a link to this nice and detailed study from Peter Vranken:

https://community.nxp.com/t5/MPC5xxx/MPC5748G-Cannot-attached-JTAG-after-erase-all/m-p/617384#M5278

Regards,

Lukas

0 Kudos
Reply

712 Views
mahoneinsh
Contributor I

Hi,lukas

Thanks for your quick reply~ 

I believe the problem was caused by reset escalation which i encountered before ,  I can always recover the board by "reset line before power on", but this time failed.

I  don't know why the program was stucked at "Verifying object file CRC-16 to device ranges..."   Then i tried to read the CFLASH data with PROGPPCNEXUS, firstly i erased the chip and it was stucked as followed pic.

mahoneinsh_0-1678503496344.png

Then i read the flash by clicking "SM Show Module", found the content are full with "XX"

mahoneinsh_1-1678503577206.png

mahoneinsh_2-1678503596130.png

 

 

 

0 Kudos
Reply

711 Views
mahoneinsh
Contributor I

The problem was solved~  I used PROGPPCNEXUS to reset the chip by clicking "RE Reset chip". Now my board can work well.

mahoneinsh_0-1678505741242.png

 

0 Kudos
Reply