S32 Design Studio for PowerPC Licensing and GCC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 Design Studio for PowerPC Licensing and GCC

跳至解决方案
1,524 次查看
michaelgoudey
NXP Employee
NXP Employee


I have installed S32DS for ARM and also have taken a look at pre-release PPC version.  Where is the license file included with this installation?  It's not at all obvious like the directory structure included with KDS.

 

I would also like to know about GCC version included with S32DS for PowerPC.  It appears to be a VLE toolchain with GCC v4.9.2.  The one included with S32DS for ARM looks like GCC v4.9.3.

 

Is the VLE toolchain a custom one, or standard GCC?  I have searched the web and it's unclear whether VLE was added to the standard GCC compiler.

 

Thanks, Michael

标签 (1)
1 解答
875 次查看
stanish
NXP Employee
NXP Employee

Hello Michael,

Actually S32DS for ARM/Power v1.0 does not require any specific license file.

S32DS Basic framework is based on GNU components (GCC, GDB, Eclipse...) similarly as e.g. KDS.

Regarding S32DS for Power - it indeed includes VLE toolchain. VLE support has been added by Freescale into standard GCC (4.9.2)

Hope it helps.

Stanislav

在原帖中查看解决方案

2 回复数
876 次查看
stanish
NXP Employee
NXP Employee

Hello Michael,

Actually S32DS for ARM/Power v1.0 does not require any specific license file.

S32DS Basic framework is based on GNU components (GCC, GDB, Eclipse...) similarly as e.g. KDS.

Regarding S32DS for Power - it indeed includes VLE toolchain. VLE support has been added by Freescale into standard GCC (4.9.2)

Hope it helps.

Stanislav

875 次查看
michaelgoudey
NXP Employee
NXP Employee

Thanks Stanislav.

This is exactly what I was looking for.  S32DS does not use a custom toolchain, and VLE has been added to standard GCC.  Can I see the support in a GCC git tree somewhere?

Regards,


Michael Goudey

0 项奖励
回复