I have installed S32DS for ARM and also have taken a look at pre-release PPC version. Where is the license file included with this installation? It's not at all obvious like the directory structure included with KDS.
I would also like to know about GCC version included with S32DS for PowerPC. It appears to be a VLE toolchain with GCC v4.9.2. The one included with S32DS for ARM looks like GCC v4.9.3.
Is the VLE toolchain a custom one, or standard GCC? I have searched the web and it's unclear whether VLE was added to the standard GCC compiler.
Thanks, Michael
解決済! 解決策の投稿を見る。
Hello Michael,
Actually S32DS for ARM/Power v1.0 does not require any specific license file.
S32DS Basic framework is based on GNU components (GCC, GDB, Eclipse...) similarly as e.g. KDS.
Regarding S32DS for Power - it indeed includes VLE toolchain. VLE support has been added by Freescale into standard GCC (4.9.2)
Hope it helps.
Stanislav
Hello Michael,
Actually S32DS for ARM/Power v1.0 does not require any specific license file.
S32DS Basic framework is based on GNU components (GCC, GDB, Eclipse...) similarly as e.g. KDS.
Regarding S32DS for Power - it indeed includes VLE toolchain. VLE support has been added by Freescale into standard GCC (4.9.2)
Hope it helps.
Stanislav
Thanks Stanislav.
This is exactly what I was looking for. S32DS does not use a custom toolchain, and VLE has been added to standard GCC. Can I see the support in a GCC git tree somewhere?
Regards,
Michael Goudey