Can anyone help me out how to convert ADC result in FIFO to voltage assume my ref is 5V and input Vin is 2.5 V. ADC resolution is 12 bit. say im reading a single channel ANA23.
. I saw the example couldnt understandit. kindly guide me.
Hi Thanks,
Ya i meant eQADC of MPC5777c. Please tell me if i give 2.5V as input 5V reference based on the equation how can i manipulate it and check whether i got back what input i gave. for diagnostic purposes i need to perform this .
The question might be trivial but i just need to check whether my understanding is right.
Thanks In Advance
theoretically you should get value 0x2000
BR, Petr
Hi,
you did not specify the MCU, but I guess you meant eQADC of MPC5777C.
If yes, then refer to table Table 30-134 of the device Reference Manual. It gives correspondence between analog voltages and digital values. From this you can see that for max input value the result in RFIFO is 0x3FFC.
So for your 5V reference the equation for input voltage in mV is
inp_mV = 5000 * RFIFO value / 0x3FFC
BR, Petr