No source available for 0x80040 in s32DS

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

No source available for 0x80040 in s32DS

ソリューションへジャンプ
3,507件の閲覧回数
dineshmoka
Contributor III

Hi I am using S32 DS and PE multilink universal debugger for MPC5777c-416DS with MPC 57xx mother board...when am running the code through debug configurations one popup window is coming showing...NO SOURCE AVAILABLE FOR 0x800400

タグ(1)
0 件の賞賛
返信
1 解決策
3,483件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This means that you are missing source code. For example if you executed some library function where is missing source code.
Or it could be refresh issue.

Try to rebuild whole project and make sure you have all source files which are required.

 

best regards,

Peter

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
3,484件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This means that you are missing source code. For example if you executed some library function where is missing source code.
Or it could be refresh issue.

Try to rebuild whole project and make sure you have all source files which are required.

 

best regards,

Peter

0 件の賞賛
返信
3,466件の閲覧回数
dineshmoka
Contributor III

Hi Peter 

Y each time this popup window is coming each time I started debugging

0 件の賞賛
返信