No source available for 0x80040 in s32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

No source available for 0x80040 in s32DS

Jump to solution
3,443 Views
dineshmoka
Contributor III

Hi I am using S32 DS and PE multilink universal debugger for MPC5777c-416DS with MPC 57xx mother board...when am running the code through debug configurations one popup window is coming showing...NO SOURCE AVAILABLE FOR 0x800400

Tags (1)
0 Kudos
Reply
1 Solution
3,419 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This means that you are missing source code. For example if you executed some library function where is missing source code.
Or it could be refresh issue.

Try to rebuild whole project and make sure you have all source files which are required.

 

best regards,

Peter

View solution in original post

0 Kudos
Reply
2 Replies
3,420 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This means that you are missing source code. For example if you executed some library function where is missing source code.
Or it could be refresh issue.

Try to rebuild whole project and make sure you have all source files which are required.

 

best regards,

Peter

0 Kudos
Reply
3,402 Views
dineshmoka
Contributor III

Hi Peter 

Y each time this popup window is coming each time I started debugging

0 Kudos
Reply