No source available for 0x80040 in s32DS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

No source available for 0x80040 in s32DS

跳至解决方案
3,444 次查看
dineshmoka
Contributor III

Hi I am using S32 DS and PE multilink universal debugger for MPC5777c-416DS with MPC 57xx mother board...when am running the code through debug configurations one popup window is coming showing...NO SOURCE AVAILABLE FOR 0x800400

标记 (1)
0 项奖励
回复
1 解答
3,420 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This means that you are missing source code. For example if you executed some library function where is missing source code.
Or it could be refresh issue.

Try to rebuild whole project and make sure you have all source files which are required.

 

best regards,

Peter

在原帖中查看解决方案

0 项奖励
回复
2 回复数
3,421 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This means that you are missing source code. For example if you executed some library function where is missing source code.
Or it could be refresh issue.

Try to rebuild whole project and make sure you have all source files which are required.

 

best regards,

Peter

0 项奖励
回复
3,403 次查看
dineshmoka
Contributor III

Hi Peter 

Y each time this popup window is coming each time I started debugging

0 项奖励
回复