Hello,
we are currently testing the external RAM of the MPC5777C-516DS using the provided example software (https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/Example-MPC5777C-External-SRAM-test-GHS714/ta-p/...). It runs fine although bursting is not enabled which we want to use for our application.
To enable bursting we changed the following settings:
EBI.CAL[0].BR.R = 0x200000C1
se_bgeni r3,2 // virtual address at 0x2000_0000
e_ori r3,r3,0x0030 // VLE, cache-enabled, write through
mtspr MAS2,r3 // Load MAS2 with 0x2000_0030 for TLB entry #2
To check if the external RAM is working we implemented a simple test:
But something peculiar happens when executing the test: Wrong data is read from the external RAM in the loop that checks for errors. When we set a breakpoint in it we also see the wrong data in the memory dump of the TRACE32-debugger. However, after the execution of the loop is finished the dump shows the correct data. This leads us to assume that the problem is caused by caching but we were unable to find a solution.
Is it possible to use burst accesses with the EVB? If yes, could you please provide the settings that have to be used for the hardware present on the MPC5777C-516DS?
Regards,
Bernd
Please create support ticket with reference to this thread:
https://www.nxp.com/support/support:SUPPORTHOME
https://www.nxp.com/video/tutorial-for-nxp-support-case-portal:NCP-VIDEO
I have some example code but not in form I could share it here.
I have browsed with old ticket database, finding several times EBI bursting should work on this device.