Hi all,
I have a short/simple question.
-The MMU entries configuration, is it one shared configuration among the both cores (core 0 and core 1) or is it a core specific configuration ?
- In case it is is a core specific configuration, could one modify the core 1 MMU entries from code executed from core 0 ?
thank you for the quick reply
Hi @ORaissouni
Each core has own MMU:
A core can acccess only own MMU. It's done via core registers (MAS0 - MAS6) and via asm instructions (like tlbwe - TLB write entry). There's no way to initialize MMU of core 1 by core 0.
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MMU-Assist-Register-CONFIGURATOR/ta-p/1110436
Regards,
Lukas