Hello.
I'm trying to use shared memory on MPC5748G.
I modified the link descriptors according to examples, and also tried to implement hardware semaphores.
However, once I attempt to write to any SEMA42 register, an IVOR1 exception is triggered.
My code is following:
int main(void)
{
xcptn_xmpl ();
peri_clock_gating(); /*Allow clk for PIT and FlexCAN*/
system160mhz();
hw_init();
SEMA42.RSTGT.W.R = 0xE200; /* IVOR1 exception thrown*/
SEMA42.RSTGT.W.R = 0x1DFF; /* Reset ALL Semaphores Gates 2nd write */
//Other code...
I must have missed something. Is any SEMA42 initialization required?
I also attempted to access the SEMA42 registers in interrupt handler, but still I received IVOR1 exception.
while(status != core_num)
{
/*Lock the gate*/
SEMA42.GATE[0].R = core_num + 1;// IVOR1 exception thrown
status = SEMA42.GATE[0].R;
}
I believe I use supervisor mode (I didn't attempt to switch modes).
Any Ideas what am I doing wrong?
Thank you and best regards, Ondra.
解決済! 解決策の投稿を見る。
Hi,
got it. It's caused by old revision of header file - there's wrong base address of SEMA42. It has been fixed in v6.0.2. You will find it attached.
But anyway, I recommend to update the S32 Design Studio. The latest update is UP8:
S32 Design Studio IDE for Power Architecture based MCUs|NXP
Regards,
Lukas
Hi,
I can't see any problem here. The SEMA42 registers can be accessed without any initialization.
I did very quick test when I locked/unlocked first two gates and then I tested the reset of gates and it works as expected. I used new empty project created in S32 Design Studio.
SEMA42.GATE[0].R = 1;
SEMA42.GATE[0].R = 0;
SEMA42.GATE[1].R = 1;
SEMA42.GATE[1].R = 0;
SEMA42.GATE[0].R = 1;
SEMA42.GATE[1].R = 1;
SEMA42.RSTGT.W.R = 0xE200;
SEMA42.RSTGT.W.R = 0x1D00;
SEMA42.RSTGT.W.R = 0xE201;
SEMA42.RSTGT.W.R = 0x1D01;
Could you share your project?
Regards,
Lukas
Hello.
Thanks for reply.
I tried to create new project with SEMA42 access only, however the result is still the same...
My previous reduced project is attached.
I use s32 2017.R1 and microcontroller MPC5748GMKU6 (version of mask 1N81M).
Could you please share your working project?
Thank you, Ondřej.
Hi,
got it. It's caused by old revision of header file - there's wrong base address of SEMA42. It has been fixed in v6.0.2. You will find it attached.
But anyway, I recommend to update the S32 Design Studio. The latest update is UP8:
S32 Design Studio IDE for Power Architecture based MCUs|NXP
Regards,
Lukas
Hello.
Thank you.
Problem solved.
Best regards, Ondřej.