Hello,
I am having problems with interrupts for the 1588 timer. Even with EIR[TS_TIMER] asserted and EIMR[TS_TIMER] unmasked, my interrupt handler is not called. I have performed and verified the following steps:
I am also fairly certain that my interrupt handler is configured correctly since I can use PSR214[SWTN] to trigger the handler manually.
Is there any additional operations that needs to be performed for the TS_TIMER interrupt to trigger the interrupt vector? I am testing on ENET0 and the system is using eCos as OS if that makes any difference.
Best regards,
Johannes
解決済! 解決策の投稿を見る。
Hi Johannes,
it looks similar as this one...https://community.nxp.com/thread/438400
Try to use vector #210 (ENET group 0)
BR, Petr
Hi Johannes,
it looks similar as this one...https://community.nxp.com/thread/438400
Try to use vector #210 (ENET group 0)
BR, Petr
Thank you Petr, I had missed that #210 was timer-related and assumed #214 was the one I needed.
BR, Johannes