MPC5748G ENET TS_TIMER interrupt

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5748G ENET TS_TIMER interrupt

Jump to solution
1,075 Views
johreh
Contributor I

Hello,

I am having problems with interrupts for the 1588 timer. Even with EIR[TS_TIMER] asserted and EIMR[TS_TIMER] unmasked, my interrupt handler is not called. I have performed and verified the following steps:

  • INTC.PSR214 register is configured (processor 0, priority 14)
  • ATPER is configured (10^9)
  • ATINC[INC] is 0x19 and ATINC[INC_CORR] is 0
  • ATCR[EN] and ATCR[PEREN] is enabled
  • I see that ATSTMP is periodically updated and I can set ATCR[CAPTURE] to read the timer register
  • EIMR[TS_TIMER] is enabled
  • I can observe in the debugger that EIR[TS_TIMER] is re-set after 1 second as expected after manually clearing the flag.
  • Other ENET interrupts are properly triggered, e.g. EIR[TXF] and EIR[RXF]

I am also fairly certain that my interrupt handler is configured correctly since I can use PSR214[SWTN] to trigger the handler manually.

Is there any additional operations that needs to be performed for the TS_TIMER interrupt to trigger the interrupt vector? I am testing on ENET0 and the system is using eCos as OS if that makes any difference.

Best regards,

Johannes

Tags (3)
0 Kudos
1 Solution
809 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Johannes,

it looks similar as this one...https://community.nxp.com/thread/438400 

Try to use vector #210 (ENET group 0)

BR, Petr

View solution in original post

0 Kudos
2 Replies
810 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi Johannes,

it looks similar as this one...https://community.nxp.com/thread/438400 

Try to use vector #210 (ENET group 0)

BR, Petr

0 Kudos
809 Views
johreh
Contributor I

Thank you Petr, I had missed that #210 was timer-related and assumed #214 was the one I needed.

BR, Johannes

0 Kudos