MPC5744P FLASH ERASE SSD C55 DRIVER ERROR

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5744P FLASH ERASE SSD C55 DRIVER ERROR

446件の閲覧回数
Ekaitz
Contributor II

I have problems when I'm doing a flash erase with the SSD C55 flash driver. 

I'm doing a bootloader so I found a CAN bootloader. So I took the example and got to run it.

But when I start modifiying to ajust for my app I can't get it to work.

I have the bootloader in this flash positions:

/*16 KB low flash memory block 2 (boot location 0) from 0x00F98000 to 0x00F9BFFF*/
/*16 KB low flash memory block 3 (boot location 1) from 0x00F9C000 to 0x00F9FFFF*/
/*64 KB low flash memory block 4 (boot location 2) from 0x00FA0000 to 0x00FAFFFF*/
/* use the low flash memory block 2 and 3(96KB in total) as bootloader area */
flash_rchw :          org = 0x00F98000,  len = 4
cpu0_reset_vec :  org = 0x00F98004,  len = 4
m_text :                  org = 0x00F98008, len = 96K - 4 - 4

So I wont to erase the rest of the momry so I configure the SSD C55 driver like that:

- block_mpc574xP.h:

#define UNLOCK_LOW_BLOCKS 0x0000000E 
#define UNLOCK_MID_BLOCKS 0x00000000
#define UNLOCK_HIGH_BLOCKS 0x00000001
#define UNLOCK_FIRST256_BLOCKS 0x00

#define SKIP_IDX_NUM 0x4

- block_mpc574xP.c:

const UINT32 SKIP_BLOCK_IDX[SKIP_IDX_NUM] =
{
    /*for bootloader project, the flash block to ship depends on the project linker command file*/
    0x1, /* BAF block */
    0x2, /* bootloader block, Flash low 1 block: address 0x00F98000 to 0x00F9BFFF */
    0x3, /* bootloader block, Flash low 2 block: address 0x00F9C000 to 0x00F9CFFF */
    0x6 /* bootloader block, Flash high 0 block: address 0x00FA0000 to 0x00FAFFFF */
};

But when I do this modification and I run the program, this is allways jumping to the  EER_exception_handler.

Someone solved this?

Thanks

Thanks

タグ(1)
0 件の賞賛
0 返答(返信)