Startup. S is a file that generates a DIAB compiler for S32DS

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Startup. S is a file that generates a DIAB compiler for S32DS

623 Views
lubo_NEW
Contributor III

222222.pngAs shown in the figure, when S32DS has DIAB installed, compile the generated startup code, STARTUP.S
/* Greenhills *//* GCC *//* Diab */ A selection appears in which other files are defined
How to define Starup. S if I use AUTOSAR\ MPC574XG_AUTOSAR \ OS_4_0_92_rtm_1_0_3 \ SSC \hwspec\diabppc?
The contents of the CRTS are taken directly as the startup file

0 Kudos
Reply
0 Replies