HI,
Can MPC5743 implement IO interrupt?
Can you send me a project example?
Hello,
Yes, it can do interrupt via IO.
Please refer to reference manual chapter 16.3.4.1 External interrupt initialization.
Futhermore the available examples are in S32DS:
and also here:
https://community.nxp.com/t5/MPC5xxx-Knowledge-Base/MPC5-software-example-list/ta-p/1102445#MPC5744P
Best regards,
Peter
HI,
Can you get back to me as soon as possible? Thank you very much
HI
Thank you very much for your reply
Can you give me a specific link to which example project it is?
Hello,
I do not know if there is a direct example for what you looking for. I have not find it.
However you can use this one instead as a guide:
https://community.nxp.com/docs/DOC-343728
The devices are very familiar, same SIUL2, same INTC.
Best regards,
Peter
Hello,
As I have said. I didn't find one directly for SPC5744P.
But you can use the SPC5748G as template. They use the same IP modules.
With little porting, it should work with no issues.
Best regards,
Peter