MPC565 erase with CW6.6 Error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC565 erase with CW6.6 Error

4,043 次查看
lucid_lucid86
Contributor I

Hi My Friends.

i am trying to erase the MPC565 (56 Mhz) with CW6.6 and i have an error that it's screen shot is attached . 

the MPC565 crystal is 20 MHz . and .cfg file is attached too .

my error is "the CFP can not write target memory at location 0x3f8000 "

my programmer is P&E USB multilinks . 

is there any one help me??

标签 (1)
0 项奖励
回复
12 回复数

2,297 次查看
amkamboj
Contributor I

Hi Lucid,

Did you read/write mpc565mzp56 after this?

0 项奖励
回复

3,916 次查看
lucid_lucid86
Contributor I

is there any one help me?

i could solve reset problem . but i can not program erase or debug yet . i have "unknown protocol error" on CW6.6

0 项奖励
回复

3,916 次查看
johnny_pe
Contributor III

Hi Lucid,


What is the voltage on your VFLASH pin?

pastedImage_1.png

Regards,

Johnny

PEMicro Support

0 项奖励
回复

3,916 次查看
lucid_lucid86
Contributor I

Hi Johnny

VFLASH is 4.95 V

0 项奖励
回复

3,916 次查看
johnny_pe
Contributor III

Hi Lucid,

The cfg that you originally attached does some configuration of the chip selects for external flash. Are you trying to program internal flash or external flash memory? Make sure you are loading the correct script for the memory.

Regards,

Johnny

PEmicro Support

0 项奖励
回复

3,916 次查看
lucid_lucid86
Contributor I

my problem is not with flash 

i can not access to CALRAM .

the MPC565 is continuously in reset mode is it normal??

0 项奖励
回复

3,916 次查看
lucid_lucid86
Contributor I

I am trying to program internal flash

0 项奖励
回复

3,916 次查看
lucid_lucid86
Contributor I

it is first time that we want run this board . the error is for CALRAM. 

B0EPEE and EPEE is high in my circuit . 

all reset pins (PORESET,HRESET,SRESET) are continuously Active . 

is there any solution for my problem???

Best Regards 

0 项奖励
回复

3,916 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

can you read the flash using a debugger? Has censorship been enabled? Did you try to use newer CodeWarrior 8.7?

Regards,

Lukas

0 项奖励
回复

3,916 次查看
lucid_lucid86
Contributor I

Hi Lukas

1- yes i can read (just read no write) flash .

2- i don't know . how can i  check it?

3-yes i try with 8.7 but it did not work  like 6.6

0 项奖励
回复

2,294 次查看
amkamboj
Contributor I

Hi Lucid,

did you read/write the mpc565mzp56?

0 项奖励
回复

3,916 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

If you can read the flash, it's not censored.

Did it work before? If yes, what were the last operations?

What about B0EPEE pin?

pastedImage_1.png

Regards,

Lukas

0 项奖励
回复