MPC565 erase with CW6.6 Error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC565 erase with CW6.6 Error

4,046件の閲覧回数
lucid_lucid86
Contributor I

Hi My Friends.

i am trying to erase the MPC565 (56 Mhz) with CW6.6 and i have an error that it's screen shot is attached . 

the MPC565 crystal is 20 MHz . and .cfg file is attached too .

my error is "the CFP can not write target memory at location 0x3f8000 "

my programmer is P&E USB multilinks . 

is there any one help me??

ラベル(1)
0 件の賞賛
返信
12 返答(返信)

2,300件の閲覧回数
amkamboj
Contributor I

Hi Lucid,

Did you read/write mpc565mzp56 after this?

0 件の賞賛
返信

3,919件の閲覧回数
lucid_lucid86
Contributor I

is there any one help me?

i could solve reset problem . but i can not program erase or debug yet . i have "unknown protocol error" on CW6.6

0 件の賞賛
返信

3,919件の閲覧回数
johnny_pe
Contributor III

Hi Lucid,


What is the voltage on your VFLASH pin?

pastedImage_1.png

Regards,

Johnny

PEMicro Support

0 件の賞賛
返信

3,919件の閲覧回数
lucid_lucid86
Contributor I

Hi Johnny

VFLASH is 4.95 V

0 件の賞賛
返信

3,919件の閲覧回数
johnny_pe
Contributor III

Hi Lucid,

The cfg that you originally attached does some configuration of the chip selects for external flash. Are you trying to program internal flash or external flash memory? Make sure you are loading the correct script for the memory.

Regards,

Johnny

PEmicro Support

0 件の賞賛
返信

3,919件の閲覧回数
lucid_lucid86
Contributor I

my problem is not with flash 

i can not access to CALRAM .

the MPC565 is continuously in reset mode is it normal??

0 件の賞賛
返信

3,919件の閲覧回数
lucid_lucid86
Contributor I

I am trying to program internal flash

0 件の賞賛
返信

3,919件の閲覧回数
lucid_lucid86
Contributor I

it is first time that we want run this board . the error is for CALRAM. 

B0EPEE and EPEE is high in my circuit . 

all reset pins (PORESET,HRESET,SRESET) are continuously Active . 

is there any solution for my problem???

Best Regards 

0 件の賞賛
返信

3,919件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

can you read the flash using a debugger? Has censorship been enabled? Did you try to use newer CodeWarrior 8.7?

Regards,

Lukas

0 件の賞賛
返信

3,919件の閲覧回数
lucid_lucid86
Contributor I

Hi Lukas

1- yes i can read (just read no write) flash .

2- i don't know . how can i  check it?

3-yes i try with 8.7 but it did not work  like 6.6

0 件の賞賛
返信

2,297件の閲覧回数
amkamboj
Contributor I

Hi Lucid,

did you read/write the mpc565mzp56?

0 件の賞賛
返信

3,919件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

If you can read the flash, it's not censored.

Did it work before? If yes, what were the last operations?

What about B0EPEE pin?

pastedImage_1.png

Regards,

Lukas

0 件の賞賛
返信