Hi,
I am using the Qorivva MPC5644A's DSPI block. The Reference Manual describes the CTAR[DBR] and talks about various clock duty cycles. The Datasheet (Rev. 7) also talks about 33/66 duty cycle at §3.17.8 DSPI timing. However, when looking at the row #4 "SCK Duty Cycle" in the "Table 48. DSPI timing", the duty cycle seems pretty fixed to 50%:
Min = ½ tSC - 2
Max = ½ tSC + 2
1) Is there a typo here and tSC should be tSCK, i.e. a reference to row #1 of the table?
2) Why is non-50/50 duty cycles described in the RM and datasheet if this tables says only 50/50 duty cycle is supported?
Indeed, a 2ns variation on the faster clock (24.4ns) gives a maximum of 42/58 duty cycle...
Thanks.
解決済! 解決策の投稿を見る。
Datasheet omits information that tSDC is only valid for 50:50 duty cycle configuration (based on DSPI_CTARn[DBR/CPHA/PBR] settings). For other SCK duty cycle configurations the absolute spec number is applied as jitter/uncertainty to the nominal high time and low time.
Datasheet omits information that tSDC is only valid for 50:50 duty cycle configuration (based on DSPI_CTARn[DBR/CPHA/PBR] settings). For other SCK duty cycle configurations the absolute spec number is applied as jitter/uncertainty to the nominal high time and low time.
Thanks. Can the documentation be corrected? (i.e. doc defect opened)
Yes, sure. I'll report it.