MPC5606s Graphic and Display

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC5606s Graphic and Display

870 次查看
tech_mofu
Contributor II

Hi,

We have chosen the mpc5606s for mid range instrumental cluster in two and three wheeler. Now need some clarification on,

1. Graphics - will mpc5606s support LVGL libraries, if not suggest which graphics libraries will be supporting for designing the instrumental in mpcs5606s.

2. Display - In datasheet it mentioned it can support up to WVGA (800X480) and in some part of the documents it is mentioned it can support only WQVGA(480X260). Which resolution it supports the maximum.

Thanks,

Vivishekh

0 项奖励
回复
3 回复数

853 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport
0 项奖励
回复

848 次查看
tech_mofu
Contributor II

Thanks. Kindly clarify point 1,

Does MPC5606s supports LVGL libraries? We use XPC560SKIT evb. If LVGL is not supported then what are the alternatives .

0 项奖励
回复

806 次查看
davidtosenovjan
NXP TechSupport
NXP TechSupport

No, it is not supported by MPC5606S.

Here is the list of supported platforms:

https://www.nxp.com/design/software/embedded-software/lvgl-open-source-graphics-library:LITTLEVGL-OP...

Graphics library for MPC5606S can be shared to customer as per NDA basis.

Please create new case with the question according procedure below:

https://community.nxp.com/t5/Using-Our-Community-Knowledge/How-to-submit-a-new-question-for-NXP-Supp...

 

If vector graphic is required, consider using of MPC5645 device, having OpenVG accelerator:

https://community.nxp.com/t5/MPC5xxx/mpc5645s-can-use-openvg/m-p/640867

... or some newer device

 

0 项奖励
回复