Hi, I'm new in Qoriwa architecture.
I'm using the MPC5606S-Demo board.
I have a problem in the TFT blacklight regulation.
I'm trying to output a PWM signal from PG12 output line. The output is every time low.
I try to output the PWM in likes PJ14 and PK0 and are working fine but when I try in lines PG12 / PK10 and PK11 doesn't work.
I'm using the code warrions IDE and the code is on bottom of the post:
I don't know what I'm doing wrong ?
Can some body help me in this problem.
Thanks in advance.
void initEMIOS_0(void)
{
ME.PCTL[72].R = 0x01; // MPC56xxB/P/S EMIOS 0: select ME.RUNPC[0]
CGM.AC1_SC.R = 0x03000000; // MPC56xxS: Select aux. set 1 clock to be FMPLL0
CGM.AC1_DC.B.DE0 = 1; // MPC56xxS: Enable aux. clock to eMIOS0
EMIOS_0.MCR.B.GPRE = 63; // Divide 64 MHz sysclk by 63+1 = 64 for 1MHz eMIOS clk
EMIOS_0.MCR.B.GPREN = 1; // Enable eMIOS clock
EMIOS_0.MCR.B.GTBE = 1; // Enable global time base
EMIOS_0.MCR.B.FRZ = 1; // Enable stopping channels when in debug mode
}
void initEMIOS_0ch23(void) // EMIOS 0 CH 23: Modulus Up Counter
{
EMIOS_0.CH[23].CADR.R = 999; // Period will be 999+1 = 1000 clocks (1 msec)
EMIOS_0.CH[23].CCR.B.MODE = 0x50; // Modulus Counter Buffered (MCB)
EMIOS_0.CH[23].CCR.B.BSL = 0x3; // Use internal counter
EMIOS_0.CH[23].CCR.B.UCPRE = 0; // Set channel prescaler to divide by 1
EMIOS_0.CH[23].CCR.B.UCPEN = 1; // Enable prescaler counter to count
EMIOS_0.CH[23].CCR.B.FREN = 1; // Freeze channel counting when in debug mode
}
void initEMIOS_0ch20(void) // EMIOS 0 CH 20: Output Pulse Width Modulation
{
EMIOS_0.CH[20].CADR.R = 250; // Leading edge when channel counter bus=500
EMIOS_0.CH[20].CBDR.R = 500; // Trailing edge when channel's counter bus=999
EMIOS_0.CH[20].CCR.B.BSL = 0x0; // Use counter bus A (default)
EMIOS_0.CH[20].CCR.B.EDPOL = 1; // Polarity-leading edge sets pin; trailing clears
EMIOS_0.CH[20].CCR.B.MODE = 0x60; // Mode is OPWM Buffered
SIU.PCR[PJ14].R = 0x0800; // Set PG12 as output with opt3
}
void initEMIOS_0ch18(void) // EMIOS 0 CH 18: Output Pulse Width Modulation
{
EMIOS_0.CH[18].CADR.R = 250; // Leading edge when channel counter bus=500
EMIOS_0.CH[18].CBDR.R = 750; // Trailing edge when channel's counter bus=999
EMIOS_0.CH[18].CCR.B.BSL = 0x0; // Use counter bus A (default)
EMIOS_0.CH[18].CCR.B.EDPOL = 1; // Polarity-leading edge sets pin; trailing clears
EMIOS_0.CH[18].CCR.B.MODE = 0x60; // Mode is OPWM Buffered
SIU.PCR[PK0].R = 0x0800; // Set PG12 as output with opt3
}
void initEMIOS_0ch15(void) // EMIOS 0 CH 18: Output Pulse Width Modulation
{
EMIOS_0.CH[15].CADR.R = 250; // Leading edge when channel counter bus=500
EMIOS_0.CH[15].CBDR.R = 750; // Trailing edge when channel's counter bus=999
EMIOS_0.CH[15].CCR.B.BSL = 0x0; // Use counter bus A (default)
EMIOS_0.CH[15].CCR.B.EDPOL = 1; // Polarity-leading edge sets pin; trailing clears
EMIOS_0.CH[15].CCR.B.MODE = 0x60; // Mode is OPWM Buffered
SIU.PCR[PK10].R = 0x0800; // Set PG12 as output with opt3
}
void initEMIOS_0ch8(void) // EMIOS 0 CH 8: Output Pulse Width Modulation
{
EMIOS_0.CH[8].CADR.R = 250; // Leading edge when channel counter bus=500
EMIOS_0.CH[8].CBDR.R = 750; // Trailing edge when channel's counter bus=999
EMIOS_0.CH[8].CCR.B.BSL = 0x0; // Use counter bus A (default)
EMIOS_0.CH[8].CCR.B.EDPOL = 1; // Polarity-leading edge sets pin; trailing clears
EMIOS_0.CH[8].CCR.B.MODE = 0x60; // Mode is OPWM Buffered
SIU.PCR[PG12].R = 0x0C00; // Set PG12 as output with opt3
}
And in Main:
initEMIOS_0();
initEMIOS_0ch23();
initEMIOS_0ch20();
initEMIOS_0ch18();
initEMIOS_0ch15();
initEMIOS_0ch8();
Solved! Go to Solution.
Hi,
take a look at reference manual, Table 9-2 on page 237:
http://www.freescale.com/files/32bit/doc/ref_manual/MPC5606SRM.pdf
Not all functions are implemented on all channels.
Best Regards,
Lukas
Hi,
take a look at reference manual, Table 9-2 on page 237:
http://www.freescale.com/files/32bit/doc/ref_manual/MPC5606SRM.pdf
Not all functions are implemented on all channels.
Best Regards,
Lukas
Thanks for the replay.
This means that the PWM name from schematic of MPC5606S-DEMO is no correctly.
I solve this problems configuring the original out as pinput and make a short (bridge with wire-rap) with a valid PWM output.
With this way I can regulate the brightness of TFT display.
Best Regards.
Miquel Soler