MPC5606S PWM output

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
1,754件の閲覧回数
miquel_soler
Contributor I

Hi, I'm new in Qoriwa architecture.

 

I'm using the MPC5606S-Demo board.

 

I have a problem in the TFT blacklight regulation.

 

I'm trying to output a PWM signal from PG12 output line. The output is every time low.

 

I try to output the PWM in likes PJ14 and PK0 and are working fine but when I try in lines PG12 / PK10 and PK11 doesn't  work.

 

I'm using the code warrions IDE and the code is on bottom of the post:

 

I don't know what I'm doing wrong ?

 

Can some body help me in this problem.

 

Thanks in advance.

 

 

 

 

 

void initEMIOS_0(void)

  ME.PCTL[72].R = 0x01;       // MPC56xxB/P/S EMIOS 0:  select ME.RUNPC[0]

  CGM.AC1_SC.R = 0x03000000;  // MPC56xxS: Select aux. set 1 clock to be FMPLL0

  CGM.AC1_DC.B.DE0    = 1;       // MPC56xxS: Enable aux. clock to eMIOS0

  EMIOS_0.MCR.B.GPRE  = 63;   // Divide 64 MHz sysclk by 63+1 = 64 for 1MHz eMIOS clk

  EMIOS_0.MCR.B.GPREN = 1;      // Enable eMIOS clock

  EMIOS_0.MCR.B.GTBE  = 1;    // Enable global time base

  EMIOS_0.MCR.B.FRZ   = 1;    // Enable stopping channels when in debug mode

}

 

void initEMIOS_0ch23(void)            // EMIOS 0 CH 23: Modulus Up Counter

{       

  EMIOS_0.CH[23].CADR.R       = 999;  // Period will be 999+1 = 1000 clocks (1 msec)

  EMIOS_0.CH[23].CCR.B.MODE   = 0x50; // Modulus Counter Buffered (MCB)

  EMIOS_0.CH[23].CCR.B.BSL    = 0x3;    // Use internal counter

  EMIOS_0.CH[23].CCR.B.UCPRE  = 0;      // Set channel prescaler to divide by 1

  EMIOS_0.CH[23].CCR.B.UCPEN  = 1;    // Enable prescaler counter to count

  EMIOS_0.CH[23].CCR.B.FREN   = 1;       // Freeze channel counting when in debug mode

}

 

void initEMIOS_0ch20(void)            // EMIOS 0 CH 20: Output Pulse Width Modulation

{       

  EMIOS_0.CH[20].CADR.R       = 250;  // Leading edge when channel counter bus=500

  EMIOS_0.CH[20].CBDR.R       = 500;  // Trailing edge when channel's counter bus=999

  EMIOS_0.CH[20].CCR.B.BSL    = 0x0;    // Use counter bus A (default)

  EMIOS_0.CH[20].CCR.B.EDPOL  = 1;      // Polarity-leading edge sets pin; trailing clears

  EMIOS_0.CH[20].CCR.B.MODE   = 0x60; // Mode is OPWM Buffered

  SIU.PCR[PJ14].R           = 0x0800; // Set PG12 as output with opt3

}

 

void initEMIOS_0ch18(void)            // EMIOS 0 CH 18: Output Pulse Width Modulation

{       

  EMIOS_0.CH[18].CADR.R       = 250;  // Leading edge when channel counter bus=500

  EMIOS_0.CH[18].CBDR.R       = 750;  // Trailing edge when channel's counter bus=999

  EMIOS_0.CH[18].CCR.B.BSL    = 0x0;    // Use counter bus A (default)

  EMIOS_0.CH[18].CCR.B.EDPOL  = 1;      // Polarity-leading edge sets pin; trailing clears

  EMIOS_0.CH[18].CCR.B.MODE   = 0x60; // Mode is OPWM Buffered

  SIU.PCR[PK0].R            = 0x0800; // Set PG12 as output with opt3

}

 

void initEMIOS_0ch15(void)            // EMIOS 0 CH 18: Output Pulse Width Modulation

{       

  EMIOS_0.CH[15].CADR.R       = 250;  // Leading edge when channel counter bus=500

  EMIOS_0.CH[15].CBDR.R       = 750;  // Trailing edge when channel's counter bus=999

  EMIOS_0.CH[15].CCR.B.BSL    = 0x0;    // Use counter bus A (default)

  EMIOS_0.CH[15].CCR.B.EDPOL  = 1;      // Polarity-leading edge sets pin; trailing clears

  EMIOS_0.CH[15].CCR.B.MODE   = 0x60; // Mode is OPWM Buffered

  SIU.PCR[PK10].R            = 0x0800; // Set PG12 as output with opt3

}

 

void initEMIOS_0ch8(void)            // EMIOS 0 CH 8: Output Pulse Width Modulation

{       

  EMIOS_0.CH[8].CADR.R       = 250;  // Leading edge when channel counter bus=500

  EMIOS_0.CH[8].CBDR.R       = 750;  // Trailing edge when channel's counter bus=999

  EMIOS_0.CH[8].CCR.B.BSL    = 0x0;     // Use counter bus A (default)

  EMIOS_0.CH[8].CCR.B.EDPOL  = 1;       // Polarity-leading edge sets pin; trailing clears

  EMIOS_0.CH[8].CCR.B.MODE   = 0x60; // Mode is OPWM Buffered

  SIU.PCR[PG12].R          = 0x0C00; // Set PG12 as output with opt3

}

 

And in Main:

  initEMIOS_0();

  initEMIOS_0ch23();     

  initEMIOS_0ch20();

  initEMIOS_0ch18();

  initEMIOS_0ch15();

  initEMIOS_0ch8();

ラベル(1)
0 件の賞賛
返信
1 解決策
1,142件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

take a look at reference manual, Table 9-2 on page 237:

http://www.freescale.com/files/32bit/doc/ref_manual/MPC5606SRM.pdf

Not all functions are implemented on all channels.

Best Regards,

Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
1,143件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

take a look at reference manual, Table 9-2 on page 237:

http://www.freescale.com/files/32bit/doc/ref_manual/MPC5606SRM.pdf

Not all functions are implemented on all channels.

Best Regards,

Lukas

0 件の賞賛
返信
1,142件の閲覧回数
miquel_soler
Contributor I

Thanks for the replay.

This means that the PWM name from schematic of MPC5606S-DEMO is no correctly.

I solve this problems configuring the original out as pinput and make a short (bridge with wire-rap) with a valid PWM output.

With this way I can regulate the brightness of TFT display.

Best Regards.

Miquel Soler

0 件の賞賛
返信