MPC5517S debug of JTAG

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5517S debug of JTAG

865件の閲覧回数
leifang
Contributor I

Hi expert,

I am working well through document AN4365 Qorivva MPC56xx Flash Programming Through Nexus JTAG. But when I debug MPC55xx using document AN3283 MPC5500 Flash Programming Through Nexus JTAG, I met some problems.

When GPR write Access, Single Step return back OnCE Status Register is 0x309, not 0x209. Before single step, the IR of cpuscr access used LWZ R31 ( 0x53FE0000 ) , it was the same with MPC56xx.

Could you give me some advices? Is it the Instruction Register (IR) right ( 0x53FE0000 ) to MPC55xx?

0 件の賞賛
返信
3 返答(返信)

860件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

if I can remember, this worked on my side on MPC55xx (testing script for Lauterbach debugger):

;scan in OCMD - select CPUSCR register
JTAG.SHIFTTMS 1 1 0 0 ;enter Shift-IR
JTAG.SHIFTREG 0 0 0 0 1 0 0 0 0 0 ;CPUSCR register (Register Select 0b001_0000, least significant bit first)
JTAG.SHIFTTMS 1 0 ;return to run-test/idle

;write CPUSCR
JTAG.SHIFTTMS 1 0 0 ;enter Shift-DR
JTAG.SHIFTTDI %Long 0x40000100 ;WBBRlow - this value will replace "X" in e_lwz instruction
JTAG.SHIFTTDI %Long 0x00000000 ;WBBRhigh
JTAG.SHIFTTDI %Long 0x00000000 ;MSR
JTAG.SHIFTTDI %Long 0x40000000 ;PC - address to some valid memory
JTAG.SHIFTTDI %Long 0x53E00000 ;IR - opcode for instruction e_lwz r31,0(X)
JTAG.SHIFTREG %Long 0x00000402 ;CTL - set FFRA bit and IRSTAT8 bit

JTAG.SHIFTTMS 1 0 ;return to run-test/idle

;call function which performs single step over instruction loaded in CPUSCR
GOSUB JTAG_SingleStep

 

Which address do you read? Do you use WBBRlow? Is FFRA set?

Did you try to read another address?

Regards,

Lukas

 

0 件の賞賛
返信

852件の閲覧回数
leifang
Contributor I

Yes, after entering to debug mode (0x209),  I set OCR, DBCR0, DBSR registers.

Then I can read CPUSCR register, the value are:

wbbrlow = 0x0
wbbrhigh =0x0
init_msr = 0x0
init_pc = 0xFFFFFFFC
init_ir = 0x79FFF064
init_ctl = 0x2

I used write_cpuscr function with your suggesting parameters or MPC56xx parameters,  single setp return back 0x309,  ERR bit error.

cpuscr_access(0x40000100, 0x0, 0x0, 0x40000000, 0x53E00000, 0x402, WR_CPUSCR);
single_step();

 

I try ram address 0x40000100,  flash address 0x0,   MIDR address 0xFFFE8004, the results were the same.

I can't find the err reason.

 

 

0 件の賞賛
返信

849件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Only one idea now - is MMU configured? Can you read those addresses using Nexus RW access?

Regards,

Lukas

 

0 件の賞賛
返信