MPC5200B detailed description of JTAG/COP/BDM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MPC5200B detailed description of JTAG/COP/BDM

1,178件の閲覧回数
ulbed
Contributor I

Hello,

I have to develop a JTAG debugger for the MPC5200B.

I've searched the publicly available documents like MPC5200B User's Manual and G2 PowerPC Core Reference Manual (G2CORERM/D). It seems that there is still missing a lot of information on the COP Module / BDM Interface and JTAG instructions for the e300 core.

I need to know how to:

  • basic control (start/stop) the CPU (e300)
  • read/write to CPU registers (GPR, PC, SP, etc.)
  • read/write to peripherals

Where can I find that information?

タグ(5)
0 件の賞賛
返信
1 返信

1,067件の閲覧回数
Pavel
NXP Employee
NXP Employee

Information about JTAG/COP interface is proprietary of NXP and is not available for general access.

This interface uses internal possibilities of processor core and this information is closed.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 件の賞賛
返信