MPC5200B detailed description of JTAG/COP/BDM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MPC5200B detailed description of JTAG/COP/BDM

958 Views
ulbed
Contributor I

Hello,

I have to develop a JTAG debugger for the MPC5200B.

I've searched the publicly available documents like MPC5200B User's Manual and G2 PowerPC Core Reference Manual (G2CORERM/D). It seems that there is still missing a lot of information on the COP Module / BDM Interface and JTAG instructions for the e300 core.

I need to know how to:

  • basic control (start/stop) the CPU (e300)
  • read/write to CPU registers (GPR, PC, SP, etc.)
  • read/write to peripherals

Where can I find that information?

0 Kudos
1 Reply

847 Views
Pavel
NXP Employee
NXP Employee

Information about JTAG/COP interface is proprietary of NXP and is not available for general access.

This interface uses internal possibilities of processor core and this information is closed.

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos