MPC 5748G EVB FlexCAN

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MPC 5748G EVB FlexCAN

607 次查看
yalamandadosaky
Contributor V

Hi All, I am using s32ds v1.2 power pc in my ubuntu , I am working on FlexCAN for mpc5748g EVB , I am able send&receive CAN messages with can0 and can1 ports. But I want use can3 and can4 as there are 8 flexcan modules available for 5748g , I checked the PIN IO sheet, there are multiple tx/rx pins for each flexcan .I have configured pj[11] and pj[12] as tx and rx respectively and connected to tx and rx pins of the can0 transceiver. But it is not working.

I have checked with other pins configuration pf[8],pf[9] and pk[5],pk[6] also. But none of them are working.

Can any one help me how to solve this issue.

0 项奖励
回复
0 回复数