I cannot find any information in the S32R274 reference manual about what output the MAXS instruction will give when in global mode. I have tried running the instruction and it does not seem to give either the expected maximum value or the index of it in the vector I am running the instruction over.
What I want to do is find both the maximum value and bin number in the output of an FFT. If MAXS is not the right instruction for this, do you have another suggestion for accomplishing what I want to do?
Hello,
I cannot find any information in the S32R274 reference manual about what output the MAXS instruction will give when in global mode.
To find the global maximum, the result of the current maximum operation is also compared with the result of the previous
maximum operation and overwrites this result, if it is larger. To find the local maximum (peak), each value is compared with its nearest neighboring values.
If MAXS is not the right instruction for this, do you have another suggestion for accomplishing what I want to do?
The MAX-S is the instruction you will use to find maxima.
What I want to do is find both the maximum value and bin number in the output of an FFT
Please refer to below section in reference manual:
Best regards,
Peter
Hi,
Sorry for the late reply.
The only thing that instruction seems to output is the maximum value, not its location in the vector.
This is the input:
This is the MAXS instruction:
0x9C000400, 0x8000A000, 0x00000101, 0x00000000,
I do some PDMA instructions before and after to load from/to SPT memory.
And this is the output:
The only thing I can see in memory is the maximum value. No bitfield indicating the location.
Hello,
Looking at your MAXs instruction I am quite confused:
0x9C000400, 0x8000A000, 0x00000101, 0x00000000
So your source address is 0x8000 and destination address is 0xA000. But you are sharing to me RAM memory screenshots. Also your INC step is 0 for both src and dest.
I am also confused about your complain about not seeing maxima bitfield. Are you not seeing it in TRAM? What is the issue?
Best regards,
Peter
Hi,
Thanks to the help from Reinhard I was able to inspect the operand RAM. Still nothing where in the vector the maximum value is. Just the maximum value.
/Regards
Mikael
Hi,
It seems like it works differently in global and local mode. You seem to run it in local mode and then it seems to give a bit vector as output. But in global mode it does not. Am I correct?
If I am correct I cannot see that I would be able to get a global maxima in local mode. Or do you have a workaround?
/Regards
Mikael
Hello,
To find the global maximum, the result of the current maximum operation is also compared with the result of the previous maximum operation and overwrites the previous result, if it is larger.
Best regards,
Peter
Hi,
So there is no way for MAX-S to report the location of the global maximum value. Just the value itself.
/Regards
Mikael
Hi,
I am using a Lauterbach debugger. As far as I know it cannot directly inspect TRAM. If you know a way to directly inspect TRAM I am very interested. So therefor I load and unload from RAM using PDMA instructions. This is the whole program. 0xDEADDEAD is replace with the RAM adresses:
uint32_t maxtest[] __attribute__ ((aligned (8))) = {
//PDMA into SPT
0xA1050400, 0xDEADDEAD, 0x80000000, 0x01000001, // [1] = input_start
//MAXS
0x9C000400, 0x8000A000, 0x00000101, 0x00000000,
// PDMA transfer of output to SRAM
// Sign extension, direct address, 24-bit complex
// PDMA OPRAM (0x9000) -> SRAM (output_start), synchronous,
// Vec len = 128 units, SKIP = 127 to overwrite range FFT
0xA1070400, 0xDEADDEAD, 0xA0000000, 0x01000001, // [9] = output_start
// Stop Cmd
0x10000000, 0x00000000, 0x00000000, 0x00000000
};
SRC_ADD_INC and DEST_ADD_INC are both 1. I have made my own dissasembler to verify.
OPCODE : 100111
IN_DATTYP : 00
PREPROC : 00
THLD_CMP : 0
IN_TAG : 0
LOC_N_ABS : 0
TAG_N_BITFLD : 0
CYC_EXTN : 0
MAXSN_EN : 0
IN_PACK : 00
IMA : 0
VEC_SZ : 0x400
SRC_ADD : 0x8000
DEST_ADD : 0xA000
SRC_ADD_INC : 0x1
DEST_ADD_INC : 0x1
MAXSN_SEL : 00
THLD_ADD : 0x0
/Regards
Mikael