Loop back for LIN bus on MPC5777M EVM board?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Loop back for LIN bus on MPC5777M EVM board?

941 Views
anishchoudhary
Contributor III

Hi,

I am testing LIN communication on MPC5777M EVM board.Here external 12V supply is necessary to test communication LIN protocol ? OR it's not necessary to supply external 12V to test LIN protocol in loop back mode ?

Tags (1)
2 Replies

811 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

for internal loopback the transceiver is not used, so there is no need to supply it.

If you want to use the transceiver, then you must supply it by 12V.

BR, Petr

811 Views
anish021
Contributor I

Hi,

For supply 12v which pin we have to use, when use GPIOs for establish connection between two LIN ports ?

0 Kudos
Reply